Same-Day Shipping in the next 3:14:08
Same-day shipping if you order in the next hours!
Need assistance? Call 1-800-715-4396
CloseFairview
 

Categories

Archives

Subscribe To Our Blog

Loading

What is a LNA (Low Noise Amplifier)

There are many cases in RF circuit design where there is a need to increase the power of a signal while avoiding adding any signal degrading characteristics. An example of this is when a mixer needs to be driven at a certain input power beyond what is available from...

read more

What is a VCO?

Voltage Controlled Oscillators (VCOs) are essential elements in a wide range of applications that require frequency variation based controllable signals. Examples of this include phase locked loops (PLLs), frequency modulators, radar, and frequency hopping remote...

read more

What is a PLL (Phase-locked-loop)?

Phase-locked-loops (PLLs) are important components in many radio communication links and test equipment that rely on quality internal signals. PLLs are used in local oscillator (LO) circuits and RF Frequency Synthesizers that are designed to maintain precision...

read more

What is an RF Connection?

Radio Frequency (RF) signals are merely any useful electromagnetic radiation within a portion of the spectrum that is compatible with available technology. These can be RF signals used for communication, sensing, or any other purpose, such as RF heating, RF plasma, or...

read more

N Type Female Connectors

The N-type coaxial connector (N-female connector) is one of the oldest standardized coax connectors and has been around since the 1940s. The N-type coaxial connector is one of the most commonly used RFconnector types with a typical frequency range from DC to 11 GHz,...

read more

Categories

Archives

Subscribe To Our Blog

Loading