The short answer is, yes. A RF splitter and combiner are the same passive network devices, and to use a splitter as a combiner, the input signals are placed in the combining ports of the splitter, where the combined output is then available at the splitter input port....
RF Power Combiners/Splitters, sometimes referred to as either RF combiners, RF splitters, or RF dividers, are a fundamental passive RF component used to combine power from multiple inputs to a single output or split RF power from one input to multiple outputs. RF...