Same-Day Shipping in the next 3:14:08
Same-day shipping if you order in the next hours!
Need assistance? Call 1-800-715-4396
CloseFairview
 
Fairview Microwave » Fairview Microwave Blog

Fairview Microwave Blog

Categories

Archives

Subscribe To Our Blog

<div class="emaillist" id="es_form_f0-p1660-n1"

N-Type Coaxial Connectors in A Nutshell

N-type Coaxial Connectors are one of the most common coaxial connector types used in wireless communication and sensing systems. This connector type has been around since the 1940s and was originally designed for military applications not exceeding 1 GHz maximum operating frequency. These coaxial connectors can be found in virtually all applications that operate below 6 GHz, though there are...

read more

What Is a Tunable Bandpass Filter?

A Tunable Bandpass Filter is a type of tunable filter that exhibits significant attenuation outside of the passband of the filter, and contains a resonant or other adjustable element that allows for the center frequency and other filter characteristics to be adjusted. Tunable bandpass filters differ from fixed bandpass filters in that there are one or more elements, often resonant elements, that...

read more

Categories

Archives

Subscribe To Our Blog

<div class="emaillist" id="es_form_f0-p1660-n3"