Same-Day Shipping in the next 3:14:08
Same-day shipping if you order in the next hours!
Need assistance? Call 1-800-715-4396
CloseFairview
 
Fairview Microwave » Fairview Microwave Blog

Fairview Microwave Blog

Categories

Archives

Subscribe To Our Blog

<div class="emaillist" id="es_form_f0-p1660-n1"

What is an RF Connection?

Radio Frequency (RF) signals are merely any useful electromagnetic radiation within a portion of the spectrum that is compatible with available technology. These can be RF signals used for communication, sensing, or any other purpose, such as RF heating, RF plasma, or even RF propulsion. RF signals can be conducted through open-air channels, space, through fluids, through the ground,...

read more

N Type Female Connectors

The N-type coaxial connector (N-female connector) is one of the oldest standardized coax connectors and has been around since the 1940s. The N-type coaxial connector is one of the most commonly used RFconnector types with a typical frequency range from DC to 11 GHz, with precision N-type connectors available that reach 18 GHz. This connector type is based on the MIL-STD-348 coaxial connector...

read more

Categories

Archives

Subscribe To Our Blog

<div class="emaillist" id="es_form_f0-p1660-n3"