Same-Day Shipping in the next 3:14:08
Same-day shipping if you order in the next hours!
Need assistance? Call 1-800-715-4396
CloseFairview
 
Fairview Microwave » Fairview Microwave Blog

Fairview Microwave Blog

Categories

Archives

Subscribe To Our Blog

Loading

What Are RF Bias Tees?

RF Bias Tees are essentially three-terminal diplexers that allow for very low frequency pass through from an input RF port to a dedicated DC port, while blocking the DC from passing to the RF output port. This assumes that the incident energy at the RF input contains both DC and RF energy. Hence, the three terminal network is a high-frequency and low-frequency input port, a low-frequency output...

read more

What Are RF Power Combiners/Splitters?

RF Power Combiners/Splitters, sometimes referred to as either RF combiners, RF splitters, or RF dividers, are a fundamental passive RF component used to combine power from multiple inputs to a single output or split RF power from one input to multiple outputs. RF Power Combiners are often used to combine the output powers of several amplifiers to realize a higher output power level than is...

read more

Categories

Archives

Subscribe To Our Blog

Loading